This ZIP file contains a Revit family for Signify : Gardco Softview SVPG Gen 3, as well as supporting files that are integral to the funciton of the family in a project.


Follow these steps and Extract these files to the following locations:


Step 1. Create a Windows File Folder in the Revit Library of your choice called "Signify".

Step 2. Create a Windows File Folder within the Signify Folder created in Step 1 called "Gardco".

Step 3. Place the un-zipped Windows product folder (e.g. "OmniSpot LED Recessed Multiple") within the Gardco Folder created in Step 2.

	(This folder contains the necessary .TXT and .CSV Type Catalog)

Step 4. Extract any <File Name>.ies files to the IES Folder, typically installed in C:\Documents and Settings\All Users\Application Data\Autodesk\<Revit release name>